Initial Drive Setup
The AKD Quick Start Guide provides details for initial drive setup. Initial drive setup consists of the following general steps:
Hardware Installation:
- Install the drive on your conductive panel and connect the Protective Earth ground.
- Connect the logic power you will need to operate all of the control logic to X1.
- Connect the motor power to X2.
- Connect the feedback to X10.
- Connect the inputs and outputs you will be using on X7 and X8.
- Bring AC power to the unit and connect AC power to X3 or X4.
The detailed requirements for each release are indicated in the release notes. In the table below, we list the different versions in which the minimum requirements have changed.
| WB Version | OS | .NET Framework | Comment |
|---|---|---|---|
| 1.14.5.x | Windows 7 (x86/x64) Windows 8 (x86/x64) Windows 10 |
4.6.1 | XP and Vista compatibility is dropped (the application will not install at all as the .NET framework is not supported by these OS). If you need to run WB on one of these OS, please use the 1.14.0.x release. |
| 1.14.0.x | Windows XP Windows Vista Windows 7 (x86/x64) Windows 8 (x86/x64) Windows 10 (x86/x64) |
4.0 | - |
| 1.8.0.x | Windows XP Windows Vista Windows 7 (x86/x64) Windows 8 (x86/x64) |
4.0 | - |
| 1.5.0.x | Windows XP Windows Vista Windows 7 (x86/x64) |
4.0 | - |
| 1.4.0.x |
Windows XP |
2.0 | - |